Examples of Use

 

Please note that CODESYS SoftMotion Win V3 is product that is subject to fees and licensing. It is not activated on all CODESYScompatible controllers. Contact the manufacturer of your controller for more informa­tion about your device.

The CODESYS SoftMotion Win V3 should be used as the runtime system. Make sure that you have started the SoftMotion variant of the runtime system. These are located in Start->Programs->3S CODESYS->CODESYS Control Win V3-> CODESYS SoftMotion Win V3 as a test version. In the case of CODESYS SoftMotion Win V3 RTE, you need a special setup.

All of the examples described in this section use the CODESYS SoftMo­tion Win V3 runtime system. If necessary, they can be converted to a SoftMotion controller of another type by means of Update device. In addition, virtual drives are used in the example. These can also be replaced by physical drives with the same names.