You define tappet paths in this table editor. A tappet path defines one or more master tappets depending on position. At the upper edge of the editor window, a horizontal axis approaches the range of the master positions. The individual tappet paths follow below.
You can switch between the table editor and the graphical editor at any time.
|
Inserts a new tappet. |
|
Deletes the tappet. |
Track ID |
ID of the tappet path All tappets of a tappet path refer to the same tappet switch (a variable of type BOOL). |
X |
Position of the tappet |
Positive pass |
Switch on/off attribute
|
Negative pass |
Switch on/off attribute
|
the tappet is assigned to a result, if it is passed from the position of the master axis in the positive (increasing master values) or negative direction. |
|
X |
Position of the tappet |
Positive pass |
Switch on/off attribute
|
Negative pass |
Switch on/off attribute
|