Blending

 

Program the blending via the inputs TransitionMode and BufferMode of the function blocks MC_MoveDirectAbsolute, MC_MoveDirectRelative, MC_MoveLinearAbsolute, MC_MoveLinearRelative, MC_MoveCircularAbsolute, and MC_MoveCrcularRelative.

CODESYS SoftMotion supports the following values for the BufferMode:

CODESYS SoftMotion supports the following values for the TransitionMode:

In the blending modes, the TransitionMode must not be equal to TMNone.

The effective dynamic limits for the axes are specified by the blending mode (low, high, previous, next) when blending.

The target point of blending is restricted to a maximum of half the dura­tion of the second motion.