Dynamic tracking

 

The integrated tracking function allows the programming of motion rela­tive to a movable product coordinate system. Tracking makes sure that the motion of the product is overlapped automatically with the motion relative to the product. In simple cases, the product is located on and moves with a conveyor belt or rotary table. However, it is also possible that the product is moved by a second robot.

Use the function block MC_SetDynCoordTransform for coupling two axis groups by means of a dynamic coordinate system. Tracking is performed in addition to a motion in a dynamically configured coordinate system. This remains active after the motion of the coordinate system has been terminated. It is terminated only after a command has been executed for a following motion in a non-dynamic coordinate system.

Because using an axis group as a master is not always ideal, CODESYS provides the additional generic block MC_SetDynCoordTransformEx. This block has the same interface as MC_SetDynCoordTransform, except for the Master input.

The Master input has the SMC_IDynamicCS interface type. This inter­face includes the GetPose method that calculates the estimated posi­tion at the defined time.

See also

Tracking for CP motion

For CP motion, the axis group necessarily follows a path. If it cannot follow the path, then it issues the error SMC_AXIS_GROUP_CPTR_CANNOT_FOLLOW and stops all axes.

The following actions are appropriate for avoiding this error: