5-Axis Transformation

 

With the 5-axis transformation, you can control kinematics that consist of three linear spatial axes (X, Y, Z) and a tool head. The tool head consists of two axes that hold the tool. A tool axis rotates about the Z axis, and the tool tilts the others according to the following scheme.

_sm_img_trafo_pou_five_axis.png

Parameter: Length of dTool = Distance from the processing point (tool tip = TCP) to the rotary axis inclination.

Control of the 5-axis transformation by five positional values:

_sm_img_trafo_pou_five_axis_zero_pos.png

Zero position

Example

For the movement is N30, the inclination axis that first points in the X direction is rotated, and it remains tilted in the negative X direction at the end of the movement.

N0 PB360 PC360 (set axis B and C in modulo mode 360)
N10 F10 FB100 FC100 (velocity in X/Y/Z: 10, in B and C 100)
N20 G0 X0 Y0 Z0 C0 B30  (start position)
N30 G1 X20 B-30 (target position)

See also