Gantry System
Gantry systems consist of two or three linear axes that are arranged at right angles.
As transformations do not have to be executed in gantry systems, the respective modules for inverse and forward transformations add only one offset to the X, Y, and Z axis in two or three dimensions.
See also