Command 'Revert', Command 'Revert project'

 

Symbol: _svn_icon_revert.png

Function: This command opens the Revert dialog. In the dialog, select the objects whose local changes should be reverted, and those that are reverted to the state of the base revision of the working copy.

Call:

If you select nothing or the main node in the device tree, then all modified objects are listed in this dialog (Revert project). If you selected one or more objects, then only the changes to this object are listed and recur­sively their sub-objects (Revert).

Dialog 'Revert'

Group externals

_cds_icon_option_activated.png: The external definitions are grouped by their external storage locations.

Keep locks

_cds_icon_option_activated.png: The lock is retained for all files that are modified by the revert command.

Select/deselect all

When external objects are deleted, CODESYS SVN cannot restore this data in SVN offline mode. The user is prompted how to proceed:

See also