Command 'Steal locks'

 

Symbol: _svn_icon_lock_steal.png

Function: This command steal the lock of the object. The Lock Message dialog opens for this purpose.

Call: Context menu: SVN

Requirement: The versioned object is locked by someone else (overlaid with the _svn_icon_lock_steal.png symbol).

Dialog 'Lock Message'

Enter the reason why you lock the object:

Lock message

Example: a.mayer had to steal the lock because the changes need to be implemented so urgently.

Recent Message

Shows message in the dialog that have already been used. There you select one in order to use the lock message.

Recursive

_cds_icon_option_activated.png: The lock is stolen by the object and all subordinate child objects.

OK

Steals the lock.

When the stolen lock is successful, the object (in the object tree) is overlaid with the _svn_icon_status_locked.png symbol.