Command 'Disconnect'

 

Function: This command deletes all connections of the current project to Subversion. Then the project is switched to a non-versioned project.

Call: Action in the Test Manager TestManager.SVN

Requirement: The CODESYS Test Manager add-on is installed.

See also