Function: This command updates the working copy of the project to another SVN repository URL. This command switches a project from one branch or tag to another.
Call: Action in the Test Manager TestManager.SVN
Requirement: The CODESYS Test Manager add-on is installed.
Switch to |
Input field for the target URL in SVN
|
See also