Command 'UpdateToHeadRevision'
Function: Updates the CODESYS project with the changes from the SVN repository.
Call: Action in the Test Manager TestManager.SVN
Requirement: The CODESYS Test Manager add-on is installed.
See also
Command 'Update to revision'