Command 'Update', Command 'Update project'

 

Symbol: _svn_icon_update.png

Function: This command commits changes in the SVN repository to the project. The update is performed with the HEAD revision.

Call:

If nothing or the main node is selected, then the entire project is updated (Update project). If one or more objects are selected, then these objects and their sub-objects are updated (Update SVN).

The following cases are possible:

If only some of the objects are updated, it may be that objects with the same name already exist. For example, this situation can come from moving objects to a folder.

For this conflict, you can react in the following ways:

See also