Dialog 'Project Settings' - 'SVN Settings'
Function: The behavior of the integrated SVN version control system is configured in this dialog.
Call: Menu bar: Project ‣ Project Settings (SVN Settings).
Requirement: A project is open.
With these settings, you can overwrite the default settings that were made in the dialog Tools ‣ Options , category SVN Settings. |
|
Merge |
Behavior for the commands Update, Merge, or Switch, when both sides (working copy and SVN repository) have changed from the base version. |
Locks |
Behavior such as CODESYS SVN objects when they are changed locally. |
Marker |
Behavior for conflicts |
Create SVN_VERSION_INFO constants for IEC access |
When you activate the option, the object is created automatically. When you deactivate the option, the object is removed from the project automatically. |
See also