Dialog 'Subversion Authentication'
The dialogs are used for authenticating the server/client connection. A server or client authentication is performed depending on the initial situation and protocol.
Overview of possible protocols and dialogs
svn://: The SVN protocol; either unencrypted or SSL/TLS encrypted
Can prompt for user name and password (even for an unencrypted connection)
Can prompt for a server certificate from the dialog for authentication in order to confirm the server if a certificate is unknown, defective, or invalid (for TLS/SSL encryption)
As an alternative or in addition to the user name and password prompt, the client can also be authenticated with client certificates (for TLS/SSL encryption). The dialogs for authentication open with the client certificate.
http://: SVN via http, unencrypted
Can prompt for user name and password
https://: SVN via http, SSL/TLS encrypted.
Can prompt for user name and password
Can prompt for a server certificate from the dialog for authentication in order to confirm the server if a certificate is unknown, defective, or invalid.
As an alternative or in addition to the user name and password, the client can also be authenticated with client certificates. The dialogs for authentication open with the client certificate.
svn+ssh://: The SVN protocol, encrypted through an SSH tunnel. SSH (Secure Shell) is the usual networking tool in Linux/Unix for accessing other computers.
Can prompt for user name and password
Prompts for server certificate in the dialog for authentication if the server is still unknown in order to be sure that it is the correct server.
Dialog for authentication with a server certificate
Initial situation: CODESYS (as a client) receives an unknown or defective server certificate.
This dialog shows information about the certificate. There you can confirm the identity of the server.
|
Authentication area |
Connection that is secured Example: https://svn repository:443 |
Certificate information (for SSL/TLS connections)
|
Host name |
Example: svn repository |
|
Thumbprint |
|
|
Valid from |
|
|
Valid to |
|
|
Issuer |
Example: 3S-Smart Software Solutions GmbH |
|
Certificate |
SSH server key information (for SSH connections)
|
Key type |
|
|
Key size (bits) |
|
|
Key thumbprint |
|
Save information to RAM |
If you restart CODESYS, then you have to accept the certificate again. |
|
Save to disk |
If you restart CODESYS, then the saved certificate is used. |
|
OK |
Authenticates and established the connection. |
Note
The certificate memory is secured cryptographically and distributed with other SVN clients.
See also
Dialog for authentication with a client certificate
Initial situation: The SVN server requires a client certificate for authentication.
In this dialog, you select the client certificate in order to confirm the identity.
|
Authentication area |
Connection that is secured Example: https://svn repository:443 |
The SSL server requires a client certificate file.
|
File |
Client certificate file |
|
Save information to RAM |
If you restart CODESYS, then you have to accept the certificate again. |
|
Save to disk |
If you restart CODESYS, then the saved certificate is used. |
|
OK |
Authenticates and established the connection. |
Dialog for authentication with a pass phrase
Initial situation: The SVN server is configured so that it demands a client certificate for authentication. The applied certificate is protected by a pass phrase.
|
Authentication area |
Connection that is secured Example: https://svn repository:443 |
A pass phrase is needed to unlock the certificate.
|
Pass phrase |
Example: *** |
|
Save information to RAM |
If you restart CODESYS, then you have to accept the certificate again. |
|
Save to disk |
If you restart CODESYS, then the saved certificate is used. |
|
OK |
Authenticates with client certificates by means of a pass phrase and establishes the connection. |
Dialog for authentication with a user name and password
Initial situation: The SVN server is configured so that it demands a user name and password for authentication.
|
Authentication area |
Connection that is secured Example: https://svn repository:443 |
|
User name |
Example: a.mayr |
|
Password |
Example: *** |
|
Save information to RAM |
If you restart CODESYS, then you have to accept the certificate again. |
|
Save to disk |
If you restart CODESYS, then the saved certificate is used. |
|
OK |
Establishes the connection and authenticates it. |