|
3S-Smart Software Solutions GmbH |
CODESYS SVN |
|
Last update: Version 4.2.2.0, September 2018 |
|
CODESYS SVN allows for the development of CODESYS projects under version control by Apache™ Subversion®. CODESYS SVN provides an SVN client integrated in CODESYS. The objects of your project are versioned in a central SVN repository.
As a rule, the SVN repository should be created in a server configuration and located on a server. For testing purposes, you can create a local SVN repository where you can access per file://.
CODESYS SVN requires a license and fee and it is available as a package. If you have installed the CODESYS SVN package, then you need a security key with a valid license connected to a USB port on your computer.