Test Manager

 

The CODESYS SVN add-on provides basic SVN commands for CODESYS Test Manager.

Notice

The CODESYS Test Manager add-on has to be installed on your development system so that you can use the commands.

Note

For more information, refer to the help of the CODESYS Test Manager add-on.