The object contains the SVN metadata of the project as global constants or variables in a variable list. It is located in the POUs view. You can specifically retrieve the data of the global constants or variables by the application. By calling specific data, you can also reduce the memory usage on the controller.
The SVN metadata is provided for this purpose, subdivided over multiple global variable lists (GVLs):
SVN_VERSION_INFO
SVN_Info_Summary
SVN_Info_SummaryW
SVN_Info_URI
SVN_Info_Revisions
SVN_Info_Flags
SVN_info_LastChange
The SVN_VERSION_INFO object is created automatically when a project is imported to a SVN repository. To do so the option Create SVN_VERSION_INFO in the dialog Import project to SVN must be activated.
Furthermore you can create the object or remove it from the project with the option Generate SVN_VERSION_INFO constants for IEC Access (Dialog Project ‣ Project Settings , category SVN Settings).
|
Name |
Data type |
Description |
|
MINREVISION |
LINT |
Lowest revision number of the working copy |
|
MAXREVISION |
LINT |
Highest revision number of the working copy |
|
PARTIAL |
BOOL |
TRUE: The working copy is incomplete. Example: Cancellation during the last update due to a network error or a checkout. |
|
MODIFIED |
BOOL |
TRUE: Local changes were made. |
|
SWITCHED |
BOOL |
TRUE: Parts of the project were branched (with the Switch command). |
|
VERSION |
STRING |
Version identification, similar to Apache™ Subversion® (subversion.exe) Example: 12:34M, means MINREVISION = 12, MAXREVISION = 34, MODIFIED = TRUE For more information, refer to the documentation for Apache™ Subversion®. |
|
CLEAN |
BOOL |
TRUE: The version is clean. This is the case when MINREVISION is equal to MAXREVISION, the working copy is complete, and non-versioned, and is was not switched. |
|
URL |
WSTRING |
SVN-URL of the project Example: https://svnserver/repository/trunk/ControlABC.project |
Note
If a controller does not support the data type WSTRING, then a compiler error is issued when accessing the object SVN_VERSION_INFO.
See also