Unsigned integer value which can be used to save the system tick and calculate the time difference. The maximum measurable time interval is calculated from the data width and the resolution of the system tick. As these values are heavily system-dependent the data width of the tick can be defined:
|
CAA.TICK |
UINT |
8 bit |
Prefix: tk Example: tkStart |
|
UINT |
16 bit |
||
|
UDINT |
32 bit |
||
|
ULINT |
64 bit |