This function of the CAA_Callback.Library serves to trigger an event in order to call one or multiple callbacks.
The function returns immediately. The callbacks will be executed in the background. For this reason the function is suitable for triggering events e.g. in interrupt service routines
eEvent |
CB.EVENT |
event |
eSource |
CB.EventSource |
event source |
dwParam |
DWORD |
parameter for the receiver of the event |
eError |
CB.Error |
error description |