Events CAA_CanL2 Library

 

Callbacks activated by CAA_CanL2.library always have the following parameters:

hDriver

CAA.HANLDE

handle (output of CL2.DriverOpen)

The event numbers  8000 – 8099 are reserved for CAN and are used in the following manner:

8000

SYNC event

8001

Pre-SYNC event

8002

Post-SYNC event

8003

TIME event

8004

Pre-TIME event

8005

Post-TIME event

8006-8009

reserved

8010-8079

reserved for  higher-ranking libraries (CANopen, DeviceNet)

8080-8099

placed at the disposal of applications