Functionblocks CAA_CiA405.Library

 

(CAA_CiA405.Library)

This chapter describes standard function blocks to access CANopen from IEC 61131-3. The function blocks described in this chapter are mandatory by means of function library needs. Optional function blocks in the sense of CANopen standardization are described too in order to assimilate all function blocks defined within DS-405. The following table can be used by IEC 61131-3 compliant systems to state the features covered.

CIA405.RECV_EMCY_DEV

mandatory

CIA405.RECV_EMCY

mandatory

CIA405.SDO_WRITE4

mandatory

CIA405.SDO_READ4

mandatory

CIA405.GET_LOCAL_NODE_ID

mandatory

CIA405.GET_STATE

mandatory

CIA405.GET_CANOPEN_KERNEL_STATE

mandatory

CIA405.NMT

mandatory

CIA405.SDO_WRITE

optional

CIA405.SDO_READ

optional