This function block will approximate the integral of the function
over the time interval between the first function call
and the actual time
:
The size of the time intervals
are integers and measured in micro seconds. The approximation is carried out by use of the explicit (lrInputvariable
) resp. implicit (lrInputvariable
) Euler method:
lrInputVariable.
|
xEnable |
BOOL |
reset (see Guideline for CAA libraries) |
|
lrInputValue |
LREAL |
function value |
|
udiTM |
UDINT |
size of time interval |
|
lrIntegral |
LREAL |
approximated value of integral |
|
xOverflow |
BOOL |
error flag (TRUE in case of an overflow occurred) |