This function will project the point
onto a straight line: thereby, the direction vector of the straight line is taken as normal vector of a plane that is moved along the line as long as it touches the point
. The intersection point of the plane with the line corresponding to this location is the projected point.
The return is a dummy of type BOOL.
|
pLine |
POINTER TO MATH.LINE_3D |
pointer on straight line |
|
pvOrig |
POINTER TO MATH.Vector3D |
pointer on point|PNG72/math_image024.png.png7| to be projected |
|
pvProj |
POINTER TO MATH.Vector3D |
pointer to projected result |