The key specified by idKey will be removed from the management in the Flat. Calling MBM.FlatTest now always will return bEnabled = FALSE. The value which had been valid before calling the function will be returned in hOldMsg and should be deallocated afterwards via MBM.MsgRelease. If up to now no value has been entered in the Flat, CAA.gc_hINVALID will be returned.
Notice
MBM.FlatEnable and MBM.FlatDisable always must be called pairwise!
hFlat |
CAA.HANDLE |
Flat Handle |
idKey |
CAA.IDENT |
Key to be activated. |
peError |
POINTER TO MBM.ERROR |
Pointer on error ID. |
hOldMsg |
CAA.HANDLE |
Handle of the latest, possibly stored message. |