This function of the CAA_MemBlockMan.Library transfers a message which is identified via hMsg to the Exchange hXChg for the purpose of transmission. In usiPrio the priority must be specified the Message should be approached with.
hMsg |
CAA.HANDLE |
Handle of the Message |
usiPrio |
USINT |
Priority with which the message should be approached. |
hXChg |
CAA.HANDLE |
Handle of the Exchange. |
eError |
MBM.ERROR |
Error ID |