MEM.HighByte (FUN)

 

This function of the of the CAA_Memory.library will return the high byte of the input word „wValue“.

Input:

wValue

WORD

Word (incl. high and low byte)

Output:

MEM.HighByte

BYTE

High byte of  wValue

Example:

wValue : WORD := 16#1234 ;

->

MEM.HighByte(wValue) = 16#12