This function of the CAA_Memory.library copies the amount of "uiNumberOfBytes" of memory from memory area "Source" to "Destination", wheras these memory areas are allowed to overlap!
In case of success, the function will return “TRUE”.
Only if "pSource" or "pDestination" are set to "0" the copying will not be carried out and the function will return “FALSE”.
pSource |
DWORD |
Address of source |
pDestination |
DWORD |
Address of target |
uiNumberOfBytes |
UINT |
Number of bytes to be copied |
MEM.Move |
BOOL |
TRUE in case of success |