Overview CAA_Callback.Library
The CODESYS runtime system provides different events for different purposes. Eack event can be assigned to an event class. Further on each event arises from a certain source. With the functionality of this library it is possible to register user specific functions to handle these events.