RTCLK.GetProperty (FUN)

 

This function of the CAA_RealTimeClock.library can be used to poll the features supported by the target system.

Input:

wProperty

WORD

Property number

Output:

dwValue

DWORD

Property value

Value

RTCLK.PROPERTY

Description

Possible Values

1

RTCLK.TIMEZONESUPPORT

Support of time zones with automatic switch between summer and winter (standard) time

0: no

1: yes