TMR.GetProperty (FUN)

 

By use of this function of the CAA_Timer.libray predefined properties of the implementation may be read out. The selection of a particular prop­erty is done by wProperty, its value will be returned by dwProperty.

Input:

wProperty

WORD

Number of property

Output:

dwProperty

DWORD

Value of property

Implementation properties of the CAA.Timer.library:

Value

Name of constanat

Signification

Values

1

TMR.gc_PropHWTIMER

Number of hardware timers available

2

TMR.gc_PropSWTIMER

Number of software timers available

200

TMR.gc_PropMinClkRes

finest clock resolution (in ns)