Command 'Add Visual Element'

 

Function: The command opens a menu containing all available visual­ization elements as menu items.

Requirement: You have configured the command in the dialog box Customize in a way that you have a call in a (any) menu.

When you select an element in the menu, the element is added in the visualization editor in the upper left corner.

See also