Visualization Element 'Waiting symbol flower'
Tag: Special controls
The element indicates that the system is busy or waiting for data.
Element name |
Example: Data_Transfer Optional Hint: Assign individual names for elements so that they are found faster in the element list. |
Type of element |
Waiting symbol flower |
The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.
X |
X coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
Y |
Y coordinate of the upper left corner of the element Specified in pixels. Example: 10. |
Width |
Specified in pixels. Example: 150 |
Height |
Specified in pixels. Example: 30 |
Note
You can also change the values by dragging the box symbols () to other positions in the editor.
See also
The properties contain fixed values for the coordinates of the point of rotation. This point of rotation is shown as the symbol. The point is used as the center for rotating and scaling.
X |
X-coordinate of the point of rotation |
Y |
Y-coordinate of the point of rotation |
Note
You can also change the values by dragging the symbols () to other positions in the editor.
The properties contain fixed values for setting colors.
Frame color |
|
Fill color |
|
Transparency |
Value (0 to 255) for defining the transparency of the selected color. Example 255: The color is opaque. 0: The color is completely transparent. |
See also
The properties contain fixed values for setting the look of the element.
Line width |
Value in pixels Example: 2 Note: The values 0 and 1 both result in a line weight of 1 pixel. If no line should be displayed, then the Line style property must be set to the option Invisible. |
Fill attributes |
The way in which the element is filled.
|
Line style |
Type of line representation
|
Note
You can assign variables in the Appearance variables property for controlling the appearance dynamically. The fixed values here are overwritten.
See also
Symbol color |
Selection of a color for the flower symbol. |
Line |
Stroke width of the lines (in pixels). |
Element property 'Absolute movement'
The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.
Movement |
||
X |
Variable (numeric data type). Defines the X position (in pixels). Example: PLC_PRG.iPos_X. Increasing this value in runtime mode moves the element to the right. |
|
Y |
Variable (numeric data type). Defines the Y position (in pixels). Example: PLC_PRG.iPos_Y. Increasing this value in runtime mode moves the element downwards. |
|
Rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle1.
The midpoint of the element rotates at the Center point. This rotation point is shown as the In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right. |
|
Interior rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees). Example: PLC_PRG.iAngle2. In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.
The rotation point is shown as the Note: If a static angle of rotation is specified in the Position ‣ Angle property, then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed. |
|
Note
You can link the variables to a unit conversion.
Note
The X, Y, Rotation, and Interior rotation properties are supported by the "Client Animation" functionality.
See also
Element property 'State variables'
The variables control the element behavior dynamically.
Invisible |
Variable (BOOL). Toggles the visibility of the element. TRUE: The element is not visible at runtime. |
Note
The Invisible property is supported by the "Client Animation" functionality.
See also
These properties are available only when you select the Preview: Support client animations and overlay of native elements option in the Visualization Manager.
You can animate a movement, a rotation, and the visibility of a visualization element.
Animation time |
Time that the element executes an animation (in milliseconds) Example: 500 |
Move to the foreground |
Property value (BOOL) TRUE: At runtime, the element is displayed in the foreground. FALSE: At runtime, the element is displayed in the layer where it was inserted in the visualization editor. |
See also
Element property 'Access rights'
Requirement: User management is set up for the visualization.
Access rights |
Opens the Access rights dialog. There you can edit the access privileges for the element. Status messages:
|
See also