System Requirements

 

Software requirements

To run EcoStruxure Machine Expert - Safety, one of the following oper­ating systems must be installed:

Hardware requirements

To run EcoStruxure Machine Expert - Safety, the following workstation requirements must be fulfilled:

Device

Minimum

Recommended

IBM compatible PC with Pentium processor

1 GHz x86 architecture

2 GHz x86 architecture

System RAM

1 GB

2 GB

Hard disk

500 MB free memory space

1 GB free memory space

Color settings

True color

Web access

Web installation and registration requires Internet access system.