To access the Web server via USB, you can download the SE RNDIS PSX TM3 Bus Coupler Connection or configure an Ethernet interface of the USB-RNDIS.
Using the SE RNDIS PSX TM3 Bus Coupler Connection
You can download the SE RNDIS PSX TM3 Bus Coupler Connection which creates an RNDIS connection automatically.
Configuring the Virtual Ethernet Link
Follow these steps to configure the Ethernet interface of the USB-RNDIS port:
|
Step |
Action |
|---|---|
|
1 |
Connect the USB cable to the PC then to the bus coupler. |
|
2 |
Open Network and sharing center on your PC. |
|
3 |
Click Change adapter settings > Remote NDIS Compatible Device > Properties. |
|
4 |
Select Internet Protocol version 4 (TCP/IPv4). |
|
5 |
Click Properties. |
|
6 |
Select Use the following IP address: oIP address: 90.0.0.2 oSubnet mask: 255.0.0.0 |
|
7 |
Click OK. |
|
8 |
Close the Properties. |
|
9 |
In the web browser, enter the IP address 90.0.0.1. Result: The Web server is displayed. |