TM5 System PCI General Overview

 

General Description

Introduction

The communication electronic modules are designed to be connected to the Modicon M258 Logic Controller and Modicon LMC058 Motion Controller ranges.

Communication Electronic Module Features

The following table shows the communication electronic module features:

Reference

Description

TM5PCRS2

TM5 interface electronic module, 1 RS232, electrically isolated

TM5PCRS4

TM5 interface electronic module, 1 RS485, electrically isolated

TM5PCDPS

TM5 interface electronic module, Profibus DP slave

NOTE:

For information on compatibility rules between PCI communication electronic modules and controllers, refer to:

oModicon M258 Logic Controller Hardware Guide,

oModicon LMC058 Motion Controller Hardware Guide.

PCI slots

The figure below shows a controller with the PCI slots:

G-SE-0002041.4.gif-high.gif

 

 

NOTE: For more information on the compatibility of the PCI electronic modules with the specific Controller references and other considerations, please see the specific Hardware Guide for your Controller.

NOTICE

ELECTROSTATIC DISCHARGE

oVerify that empty PCI slots have their covers in place before applying power to the controller.

oDo not touch an exposed PCI connector.

Failure to follow these instructions can result in equipment damage.

For more details about addition of one more module, refer to Inserting the electronic Modules.