FUNCTION_BLOCK CrossProductNormed
This function will calculate the Cartesian product of two vectors . The result will be returned in vector
.
Keep in mind that, due to rounding errors, the input of two collinear vectors will not necessarily result in the null vector.
InOut: |