CAA Technical Workgroup
CAA Real Time Clock Extern
3.5.10.0
Intern|CAA|System
RTCLK
3S - Smart Software Solutions GmbH
CAA RTCLK
Vendor specific library for real time clock access.
CAA Real Time Clock
Enums
Function Blocks
Functions
GlobalConstants
Structs
GetSupplierVersion (FUN)
VersionConstants (GVL)
[1]
Based on CAA_RealTimeClock_Extern.library, last modified 01.01.1601, 00:53:00. LibDoc 3.5.16.0
The content file CAA_RealTimeClock_Extern.clean.json was generated with CODESYS V3.5 SP10 Patch 2 on 17.05.2017, 14:27:42.