UserMgrHasUserAccessRights (FUN)

FUNCTION UserMgrHasUserAccessRights : RTS_IEC_RESULT

Checks user access rights on the specified object (authorization)!

InOut:

Scope

Name

Type

Comment

Return

UserMgrHasUserAccessRights

RTS_IEC_RESULT

Error code
  • ERR_OK: If user has the requested rights on the object or if no user management is configured

  • ERR_PARAMETER: If user is not available or the object does not exist

  • ERR_FAILED: If something failed retrieving the access rights

  • ERR_NO_ACCESS_RIGHTS: Explicitly denied rights

  • ERR_INVALID_HANDLE: hUser is invalid or unknown

Input

pszObject

REFERENCE TO STRING

Full object name (see object tree)

hUser

RTS_IEC_HANDLE

Handle to the user

ulRequestedRights

DWORD

Requested rights on that object