DP_DIAG (STRUCT)

TYPE DP_DIAG : STRUCT

Data structure containing DP Slave diagnosis data (see: RDIAG).

(see IEC 61158-6)

InOut:

Name

Type

Comment

status1

IIoDrvProfibus.DP_StationStatus1

DP station status 1

status2

IIoDrvProfibus.DP_StationStatus2

DP station status 2

status3

IIoDrvProfibus.DP_StationStatus3

DP station status 3

Diag_Master_Add

USINT

address of the DP-master (Class 1) which has parameterised this DP-slave (255 means invalid or no parameterisation).

Ident_Number

UINT

Ident Number of DP slave

ExtDiag

ARRAY [0..235] OF BYTE

Extended Diagnosis Data