SALARM (FB)

FUNCTION_BLOCK SALARM

A Field Device can generate alarms to its associated Host Controller to inform it e.g. about certain process events or other events to state there are some limitations of the capabilities of the Field Device for diagnostic reasons. The Host application may use the RALARM function block to receive these alarms.

The ID parameter identifies the slot of the Field Device the alarm is generated for. The ATYPE input shall contain the alarm type. The ASPEC input shall contain the alarm specifier. The LEN input contains the length in byte of the additional alarm information stored in the AINFO parameter.

The Variable given as AINFO parameter shall be at least of LEN byte.

If the alarm is transmitted successfully, the VALID output indicates that the alarm was received by the Host Controller.

If an error occurred, the ERROR output indicates an error and the STATUS output contains the error code.

Code-Example

PROGRAM SendAlarm
VAR
    sender : CommFB.SALARM;
    alarmPayload : ARRAY[0..3] OF BYTE := [0, 1, 2, 3];     // encoding for Profinet: USI (UInt16), ARRAY[0..n] OF BYTE;
    ID : DWORD := CommFB.Constants.INVALID_ID;
END_VAR

ID := CommFB.SUBSLOT_ID(EN := TRUE, ID := PN_Device.DeviceID, SLOT := 2, SUBSLOT := 1);
sender.ID := ID;
sender.ATYPE := ProfinetCommon.AlarmType.PROCESS;
sender.ASPEC := 0;      // 0 for process-alarm
sender.LEN := SIZEOF(alarmPayload);
sender.AINFO := ADR(alarmPayload);
sender();

IF(sender.DONE OR sender.ERROR) THEN
    sender(REQ := FALSE);
END_IF
InOut:

Scope

Name

Type

Comment

Input

REQ

BOOL

The function is invoked when the REQ input is equal to 1.

ID

DWORD

Handle of the slot of the alarm source

ATYPE

UINT

Type of the alarm

ASPEC

UINT

Specifier of the alarm

LEN

UINT

Length of AINFO data in bytes

AINFO

POINTER TO BYTE

Additional alarm information

Output

DONE

BOOL

Indicates that the alarm was received by the Host Controller

BUSY

BOOL

FB is busy

ERROR

BOOL

Error detected

STATUS

DWORD

Last detected status