|
DISABLED
|
0
|
Disabled in device tree.
|
|
NOT_CONFIGURED
|
|
State after download going on with
|IP_CONFIG| after setting values to default.
|
|
IP_CONFIG
|
|
Setting IP address and port.
|BUS_ERROR| if IP address not valid. Going on with
|ENCAPSULATION_CONFIG| if ok.
|
|
ENCAPSULATION_CONFIG
|
|
Opens the TCP port to the client and if ther is no error go on
|LIST_SERVICES|, else
|BUS_ERROR|.
|
|
LIST_SERVICES
|
|
Empty state going on with
|REGISTER_SESSION|.
|
|
REGISTER_SESSION
|
|
Register Session message is send and response is evaluated. If error
|BUS_ERROR|, else
|PARAMETER_CONFIG|.
|
|
PARAMETER_CONFIG
|
|
UserParameters are going to be sent. If error accrued, a logmessage is generated and no matter what the next state is AdapterState.CONFIGURED.
|
|
CONFIGURED
|
|
Forward Open is processed here going on with
|RUNNING| if success and join multicast address if necessary, else retrying Forward Open in this state.
|
|
RUNNING
|
|
All connections established. IO data will be sent to the slave.
|
|
RESET
|
|
Performing a reset triggered on the input of the RemoteAdapter.
|
|
RESET_SERVICE
|
|
Reset service of CIP is triggered over the network.
|
|
CONNECTIVITY_CHECK
|
|
if AUTO_RESET in the configurator is enabled and the connection is lost, this states is getting active and checks, if the adapter is avaiable.
|CONFIGURED| is the next state, if the adapter is available again.
|
|
BUS_ERROR
|
|
If connection is lost and AUTO_RESET is disabled in the configurator or problems with sockets occurred, this state gets active.
|
|
ERROR
|
|
Downloaded parameter are inconsistent or no memory or connection problems
|