IoDrvEtherNetIPAdapter (FB)

FUNCTION_BLOCK IoDrvEtherNetIPAdapter EXTENDS IoDrvBase IMPLEMENTS IAdapter, CIP_Object.ICIPProvider, ICmpIoDrvParameter

Is the FB generated from the device. To see which CIP objects are implemented download ENIP_Adapter_Objects.xls Driver FB: Don´t create this FB directly.

InOut:

Scope

Name

Type

Comment

Input

xReset

BOOL

Rising Edge: Reset this IoDrvEtherNetIPAdapter instance.

Output

eState

ADAPTERSTATE

State of the EtherNet/IP Adapter see ADAPTERSTATE

eError

ERROR

Specifies the error, if adapter is in error state see ERROR