DCP_SetData (STRUCT)

TYPE DCP_SetData : STRUCT

DCP-Data that can be written to a Profinet device.

InOut:

Name

Type

Comment

Options

DCP_SetOptions

specify DCP Options that shall be stored.

IPSettings

IPParameterValue

IPSettings_SavePermanent

BOOL

The value shall be reset to its default value after a power off / power on cycle.

The value shall still be available after a power off / power on cycle.

StationName

STRING(240)

StationName_SavePermanent

BOOL

The value shall be reset to its default value after a power off / power on cycle.

The value shall still be available after a power off / power on cycle.