SubmoduleDiagnosisEntry (STRUCT)

TYPE SubmoduleDiagnosisEntry : STRUCT

Diagnosis entry for a submodule

InOut:

Name

Type

Initial

Comment

ChannelNumber

UINT

16#8000

The channel number of the diagnosis source (0x8000 means the whole submodule)

ChannelProperties

ChannelProperties

Additional channel data, not used for diagnosis that affect the whole submodule.

Diagnosis

ChannelDiagnosisData

The diagnosis-data entry