METHOD LoadRecipe : DWORD
Loads a recipe from the standard recipe file
The standard recipe file name is <recipe>.<recipedefinition>.<recipeextension>.
Entries in the recipe that do not include value assignments are not loaded and written. Refer to the "Load and write Recipe" command.
InOut: |
|