RecipeManCommands.ReadAndSaveRecipe (METH)

METHOD ReadAndSaveRecipe : DWORD

Reads the current PLC values into the recipe and afterwards stores the recipe into the standard recipe file

The content of an existing file will be overridden.

InOut:

Scope

Name

Type

Comment

Return

ReadAndSaveRecipe

DWORD

Possible last error values:

See ReturnValues (GVL) for a description of all possible errors.

Input

RecipeDefinitionName

STRING

Name of the recipe definition

RecipeName

STRING

Name of the recipe