RecipeManCommands.SaveRecipe (METH)

METHOD SaveRecipe : DWORD

Stores the recipe into the standard recipe file

The content of an existing file will be overridden. The standard recipe file name is <recipe>.<recipedefinition>.<recipeextension>.

InOut:

Scope

Name

Type

Comment

Return

SaveRecipe

DWORD

Possible last error values:

See ReturnValues (GVL) for a description of all possible errors.

Input

RecipeDefinitionName

STRING

Name of the recipe definition

RecipeName

STRING

Name of the recipe