class
IScriptApplicationExtension.
IScriptApplicationExtension
Bases: object
Scripting API to extend the application script object.
code_analysis
Access to code_analysis scripting API.
application_build_properties
Gets the application build properties of the application.
reset_memory_reserve_for_online_change
reset_pool_objects=False
Resets the memory reserve for online change of the function blocks in this application.
reset_pool_objects (bool) -- If set to True also resets the function blocks in the pool. (This parameter is optional, default = False).
reset_persistent_variables
Resets persistent variables of the application.
get_multicarrier_configuration
Gets or creates a Multicarrier configuration object
Returns an IScriptMulticarrierObject
IExtendedObject