SMC_BlockSearchPos (STRUCT)

TYPE SMC_BlockSearchPos : STRUCT

InOut:

Name

Type

Comment

dRelPosInObj

LREAL

Relative position in the path element. Range of values: 0..1

iSourceLine_No

DINT

0-based line number of the source file

iSubElement

INT

Number of elements with the same iSourceLine_No, 0-based

xPosStored

BOOL

TRUE: Position has been stored