FUNCTION SMC_GetObj : POINTER TO SMC_GEOINFO
Returns the n-th object of an SMC_OUTQUEUE. For N=0 the first element will be returned. If the number of elements is less than n+1, zero is returned.
task-safety: call from consumer task only
Scope
Name
Type
Comment
Input
poq
POINTER TO SMC_OUTQUEUE
The out queue
N
UINT
Index of object in the queue. Counting is started with N=0 for the first element.
Return
SMC_GetObj
POINTER TO SMC_GEOINFO